Real Time

PUCCH Common (Basic LTE-A FDD Uplink)

Additional Uplink parameters are described in Cell Parameters (Basic LTE-A FDD Uplink, PUSCH Common (Basic LTE-A FDD Uplink), and Sounding Reference (Basic LTE-A FDD Uplink).

3. PUCCH Common

Set PUCCH Auto-calculate per-slot params

PUCCH Auto-calculate per-slot params

N_RB(2)

N_CS(1)

nPUCCH(1)

nPUCCH(2)

nPUCCH(3)

Delta Shift PUCCH

Set PUCCH Auto-calculate per-slot params

Click this cell and then the button to open the Configure PUCCH Auto-calculate window where you can set PUCCH Common parameters, including Cyclic Prefix.

PUCCH Auto-calculate per-slot params

Displays the state for automatic calculation of per-slot parameters. To change the displayed state, refer to Set PUCCH Auto-calculate per slot params above.

N_RB(2)

Displays one of the values used for generating and mapping PUCCH (see 3GPP TS36.211). To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

N_CS(1)

Displays one of the values used for generating and mapping PUCCH (see 3GPP TS 36.211). To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

nPUCCH(1)

Displays the value of nPUCCH(1) which is used for generating and mapping PUCCH (see 3GPP TS36.211).

This parameter is valid only when PUCCH Auto-calculate per-slot params is set to on.

To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

nPUCCH(2)

Displays the value of nPUCCH(2) which is used for generating and mapping PUCCH (see 3GPP TS36.211).

This parameter is valid only when PUCCH Auto-calculate per-slot params is set to on.

To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

nPUCCH(3)

Displays the value of nPUCCH(3) which is used for generating and mapping PUCCH Format 3/3 Short for each subframe (see 3GPP TS36.211).

This parameter is valid only when PUCCH Auto-calculate per-slot params is set to on.

To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.

Delta Shift PUCCH

Displays one of the values used for generating and mapping PUCCH (see 3GPP TS36.211).

This parameter is valid only when PUCCH Auto-calculate per-slot params is set to on.

To change the displayed value, refer to Set PUCCH Auto-calculate per slot params above.